DIO#.DIR
Description
Sets or whether the bi-directional IO is an input or output.
Value | Description |
---|---|
0 | The bi-directional IO is treated as an input signal |
1 | The bi-directional IO is treated as an output signal |
Examples
Context
For more information see Digital Inputs and Outputs.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 0 to 1 |
Default Value | 0 (input) |
Data Type | Integer |
See Also | |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
DIO1.DIR | 0x368A | 0x1 | USINT | - | - | RW | False |
DIO2.DIR | 0x368B | 0x1 | USINT | - | - | RW | False | |
DIO3.DIR | 0x368C | 0x1 | USINT | - | - | RW | False | |
DIO4.DIR | 0x368D | 0x1 | USINT | - | - | RW | False | |
DIO5.DIR | 0x368E | 0x1 | USINT | - | - | RW | False | |
DIO6.DIR | 0x368F | 0x1 | USINT | - | - | RW | False |